無停電電源装置|Japan
These are navigation links to move inside this page.
FAQ
1台のパソコンで複数のモデムを使いたい。
対象機種 モデム全般
次のいずれかの方法により、1台のパソコンで複数のモデムをご利用いただけます。
(a)シリアルポート(通信ポート)が2つ以上あるパソコンの場合
ME5614E2やME5614D2などのシリアルポート用のモデムを複数台、それぞれパソコンにインストールします。
(b)シリアルポート(通信ポート)が1つとUSBポートがいくつかあるパソコンの場合
ME5614E2やME5614D2などのシリアルポート用モデムと、ME56PS2WSなどのUSBポート用モデムを1台ずつ用意し、それぞれパソコンにインストールします。
(c)シリアルポートがなくUSBポートが2つ以上あるパソコンの場合
市販のUSB-シリアル変換アダプタを使います。上記の(b)と同じ状態になりますので、(b)と同様に、ME5614E2やME5614D2とME56PS2WSなどをそれぞれパソコンにインストールします。