無停電電源装置|Japan
These are navigation links to move inside this page.
FAQ/よくあるご質問
BN-Tシリーズ[BN300T,BN220T,BN150T,BN100T,BN75T,BN50T]において、接点信号入出力カードSC07をSC05互換モードとして使用する場合の設定方法を教えてください
ジャンパー設定をすることにより接点信号入出力カード「SC05/SC06」のコネクタピン配置に変更することができます。
接点信号入出力カードのJP2〜JP9のジャンパー設定(8個)を「SC05/06」側へ変更してください。
注1:JP10は「SC05/06/07」側のままご使用ください。
注2:出荷時設定は、JP2~JP9:SC07側、JP10:SC05/06/07側です。