無停電電源装置|Japan
These are navigation links to move inside this page.
FAQ
MR1000 NTT東日本フレッツ・ドットネットの接続設定例を教えてください。
対象機種 MR1000
MR1000のフレッツ・ドットネットの接続設定例
MR1000で、NTT東日本の FLET’S.Netに接続する設定例です。
以下の設定例(1)は、 MR1000のLAN0ポートにADSLモデム、LAN1ポートにパソコンを接続し、IPv6ブリッジ及びPPPoEマルチセッションの設定を行う事により、FLET’S.Net、インターネット常時接続、FLET’S SQUARE 常時接続の併用を実現しています。
設定例(2)は、 MR1000のLAN0ポートにADSLモデムを接続し、LAN1、LAN2、LAN3ポートそれぞれで異なるIPセグメントをDHCPで払出し、それぞれがIPv6ブリッジ及びPPPoEマルチセッションを可能な設定にして、各セグメントのPCから、FLET’S.Net、インターネット常時接続、 FLET’S SQUARE 常時接続の併用を実現しています。
設定例と合わせて取扱説明書をご参照ください。
取扱説明書のダウンロードはこちら
■設定例(1): FLET’S.Net、FLET’S SQUARE、インターネット接続を併用する設定例
config例 |
説明 |
---|---|
lan 0 mode auto lan 0 mdi mdix lan 0 bridge use on lan 0 bridge group 1 lan 1 mode auto lan 1 mdi mdix lan 1 ip address 192.168.100.1/24 3 lan 1 ip dhcp service server lan 1 ip dhcp info dns 192.168.100.1 lan 1 ip dhcp info address 192.168.100.2/24 253 lan 1 ip dhcp info time 1d lan 1 ip dhcp info gateway 192.168.100.1 lan 1 bridge use on lan 1 bridge group 1 remote 0 name internet remote 0 mtu 1454 remote 0 ap 0 name ISP-1 remote 0 ap 0 datalink bind lan 0 remote 0 ap 0 ppp auth send xxxxx@xxxx.com xxxxx remote 0 ap 0 keep connect remote 0 ppp ipcp vjcomp disable remote 0 ip route 0 default 1 0 remote 0 ip nat mode multi any 1 5m remote 0 ip msschange 1414 remote 1 name Square remote 1 mtu 1454 remote 1 ap 0 name ISP-2 remote 1 ap 0 datalink bind lan 0 remote 1 ap 0 ppp auth send guest@flets guest remote 1 ap 0 keep connect remote 1 ppp ipcp vjcomp disable remote 1 ip nat mode multi any 1 5m remote 1 ip msschange 1414 syslog pri error,warn,info syslog facility 23 telnetinfo autologout 5m time zone 0900 consoleinfo autologout 8h proxydns domain 0 any * any on 0 off proxydns domain 1 any *.flets any on 1 on proxydns address 0 any on 0 off bridge 1 ip6 routing off env KANJI=SJIS |
LAN0とLAN1をブリッジグループ1としています。 remote 0 は、インターネット常時接続の設定です。 remote 1 は、FLET’S SQUARE 常時接続の設定です。 proxydns設定で、インターネットや FLET’S SQUARE の名前解決を可能にします。 IPv6ブリッジを可能にします。 |
※注1: | LAN1ポートにハブを接続して複数台のPCを接続することも可能です。この場合、MDI/MDIXの切替え設定を行う必要がある場合があります。( lan 1 mdi mdix 又は lan 1 mdi mdi ) |
config例 |
説明 |
---|---|
lan 0 mode auto lan 0 mdi mdix lan 0 bridge use on lan 0 bridge group 1 lan 1 mode auto lan 1 mdi mdix lan 1 ip address 192.168.100.1/24 3 lan 1 ip dhcp service server lan 1 ip dhcp info dns 192.168.100.1 lan 1 ip dhcp info address 192.168.100.2/24 253 lan 1 ip dhcp info time 1d lan 1 ip dhcp info gateway 192.168.100.1 lan 1 bridge use on lan 1 bridge group 1 lan 2 mode auto lan 2 mdi mdix lan 2 ip address 192.168.110.1/24 3 lan 2 ip dhcp service server lan 2 ip dhcp info dns 192.168.110.1 lan 2 ip dhcp info address 192.168.110.2/24 253 lan 2 ip dhcp info time 1d lan 2 ip dhcp info gateway 192.168.110.1 lan 2 bridge use on lan 2 bridge group 1 lan 3 mode auto lan 3 mdi mdix lan 3 ip address 192.168.120.1/24 3 lan 3 ip dhcp service server lan 3 ip dhcp info dns 192.168.120.1 lan 3 ip dhcp info address 192.168.120.2/24 253 lan 3 ip dhcp info time 1d lan 3 ip dhcp info gateway 192.168.120.1 lan 3 bridge use on lan 3 bridge group 1 remote 0 name internet remote 0 mtu 1454 remote 0 ap 0 name ISP-1 remote 0 ap 0 datalink bind lan 0 remote 0 ap 0 ppp auth send xxxxxx@xxxx.xx.jp xxxxxxx remote 0 ap 0 keep connect remote 0 ppp ipcp vjcomp disable remote 0 ip route 0 default 1 0 remote 0 ip nat mode multi any 1 5m remote 0 ip msschange 1414 remote 1 name Square remote 1 mtu 1454 remote 1 ap 0 name ISP-2 remote 1 ap 0 datalink bind lan 0 remote 1 ap 0 ppp auth send guest@flets guest remote 1 ap 0 keep connect remote 1 ppp ipcp vjcomp disable remote 1 ip nat mode multi any 1 5m remote 1 ip msschange 1414 syslog pri error,warn,info syslog facility 23 telnetinfo autologout 5m time zone 0900 consoleinfo autologout 8h proxydns domain 0 any * any on 0 off proxydns domain 1 any *.flets any on 1 on proxydns address 0 any on 0 off bridge 1 ip6 routing off env KANJI=SJIS |
LAN0、LAN1、LAN2、LAN3 をブリッジグループ1としています。 LAN1、LAN2、LAN3 のネットワークをそれぞれ 192.168.100.0/24、192.168.110.0/24、192.168.120.0/24 とし、接続するノードにDHCPでIPを配布します。 remote 0 は、インターネット常時接続の設定です。 remote 1 は、FLET’S SQUARE 常時接続の設定です。 proxydns設定で、インターネットや FLET’S SQUARE の名前解決を可能にします。 ブリッジグループ1でIPv6ブリッジを可能にします。 |