Web IME
Character Input Technology
Web IME
An HTML-based IME that can be embedded
in web content. The keyboard can also be uniquely
customized according to web content.
- Point 1
-
Embed in
web content!
- Point 2
-
Specialize keyboard
to match content
- Point 3
-
Works with various
browsers, devices, OS
What is Web IME?
- An HTML-based IME that runs in a web browser
- It is constructed using HTML and JS, so it can be embedded into web content (not including binary modules)
- Prediction and conversion can be performed using Cloud Wnn
What Web IME Can Do
- Display specialized keyboards within content
Keyboards set for each text input field can be displayed.
In addition to a QWERTY array, specialized keyboards can be displayed to match content.

- Key input
The same key input as normal IMEs is possible by tapping on the touch panel or clicking the mouse button

- Moving the keyboard
By dragging the black bar at the top of the keyboard, the display position can be changed as desired.
However, controls are in place so that the keyboard does not protrude beyond the web page (browser window)

- Cursor control
Supports automatic or manual cursor movement between multiple text fields
- Automatic cursor movement
- When inputting the specified maximum number of characters, the cursor automatically moves to the next field. (Will not move unless "Next" is specified)
- If there are no characters, you can return to the previous field using the [Delete] key.
- Manual cursor movement
- The cursor can be moved manually even if the maximum number of characters has not been entered by pressing the [Left/Right] or [Enter] keys.
- Cloud conversion
Conversion
When pressing the [Conversion] key, conversion candidates are received from the server according to the input content and displayed.
- Limitations
- Continuous passage conversion can only be obtained as one candidate. (Cloud Wnn side not yet supported)
- Scrolling is not possible even if the candidate window is expanded. (Not implemented)

Prediction
As with normal IMEs, prediction candidates corresponding to input characters are displayed.
Web IME Specifications
System configuration

Operating browser (checked browsers only)
- Chrome (confirmed working with version 42)
- Firefox (confirmed working with version 37)
- IE (confirmed working with version 9 and later)
- Safari
Operating OS (checked operating systems only)
- Windows 7
- Linux (Ubuntu)
- Mac OS
- Android (4 and later)
- Firefox OS
Click for product inquiries and questions
welcome
- corporate customer
-
Contact
Please select "Character input technology"
+81-3-6718-3712
(Japanese language only)
+81-3-6718-3713Business hours: 9:00-17:30
(except Saturdays, Sundays and public holidays)
Personnel Division:Life Infrastructure Solution Division UX Solution Department
Shinagawa Front Building 7F, 2-3-13, Konan, Minato-ku, Tokyo 108-0075, Japan